Go to description Go to description Go to description

Test Model Wizard (Advanced LTE-A Pro NB-IoT)

Click the Test Model Wizard button in the Downlink node to access the Test Model Wizard.

System Bandwidth

Displays the system bandwidth for Narrowband Test Model. (N-TM).

Test Model Type

Displays Narrowband Test Model Type.

See 3GPP TS 36.141 6.1.3 and 6.1.4 for more information.

Narrowband Cell ID

Choice: 103 | 109 | 115 | 121 … 485 | 491 | 497 | 503

Default: 103

Double-click or use the drop-down menu to set Narrowband Cell ID for Narrowband Test Mode.

See 3GPP TS 36.141 6.1.3 and 6.1.4 for more information.